Other Parts Discussed in Thread: THS4271, INA143, LM7705, TLV9002, OPA310
Tool/software:
Hi!
Need verificaion if the op-amp INA105 will suffice in my design.
- Using PicoLog ADC 24 for measuring a voltage regulated "PID" card (old school equipment ASEA) -15 - 15 VDC.
- Voltage divider 15VDC -> 2.5VDC (Max input voltage for the A/D converter is 2.5V)
- Problem: the AD converter has 24 inputs and have a low impedance input. The number og of input levels can drift the voltage significantly. Also, here is too much current being drawn from the cards. The voltage dividers makes the Data Logger inputs become even lower in resistance in comparison to the divider. By adding a inti gain buffer should take care of this problem, however my knowledge of OP-AMPS are limited.
Critera:
- Gain ratio 1/1V
- Package type DIP
I have been recommended the THS4271 chip, however this chip i waaay to small to hand solder.
See also pdf-file for overview
Best regards
Richard Møller
OPAMP_INA105-Voltagedivider with unity gain buffer for AD converter.pdf