Tool/software:
Hi,
In the AMC3302 datasheet, section 6.9, the IDD Low-side supply current is 42 mA (max) (section 6.5, maximum power dissipation: 231mW). Also in Section 6.8, the Is safety input, output or supply current is 309mA (VDD = 5.5V) (safety input, output or total power: 1700mW).
Any supply current above 309mA or power dissipation above 1700mW will damage the isolation barrier and damage the low side circuit. Do we need to use any SMD fuse in the power supply lines to protect the isolation barrier damage?
Could you please recommend the suitable fuse ratings for the high side and low side circuit?
Thanks & regards,
Ilamparithi Tamizhanangu