Tool/software:
Hello,
I am designing a single cell charger and I have used INA381 to detect when the output consumes more than 50mA of current. Could you review the design I made regarding INA381A4 and comment if it is ok, or if there are any issues? INA381 is in the part labeled "Camera status indicator".
The sole purpose of INA 381 is to turn on the red LED D5 when the current through the shunt R13 is over 50mA.
Thanks!
Samo