Other Parts Discussed in Thread: OPA863A, OPA2863, TINA-TI
Tool/software:
Hello Team,
The OPA863A (OPA2863A) model has the usual VNSE_ voltage noise and and FEMT_ current noise entries. But in addition it has a duplicate current noise entry, on the - input:
X_I_NN ESDN MID FEMT_OPA2863A PARAMS:
X_I_NN1 ESDN MID FEMT2_OPA2863A PARAMS:
In addition there are three resistors, that are not noiseless, also providing noise:
*R_R183 is NOT noiseless
R_R183 N1566688 MID 1E12
E_E1 N1566698 MID N1566688 MID 1.429E3
R_RL10 N1566698 N1566638 R_NOISELESS 10E3
C_C38 N1566698 N1566638 4.547E-11
R_RL11 N1566638 MID R_NOISELESS 7.005
E_E7 N1566868 MID N1566638 MID 5
R_RL12 N1566868 N1566646 R_NOISELESS 10E3
C_C39 N1566868 N1566646 1.592E-13
R_RL13 N1566646 MID R_NOISELESS 2.5E3
G_G82 NOISE_OUT MID N1566646 MID 1E-10
*R_R182 is NOT a noiseless resistor!
R_R182 N1548704 MID 1E12
G_G78 N1548814 MID N1548704 MID -1.75E-4
R_RL1 N1548814 MID R_NOISELESS 1
R_RL3 N1548814 N1548992 R_NOISELESS 10E3
C_C36 N1548814 N1548992 7.958E-13
R_RL4 N1548992 MID R_NOISELESS 7.407E3
G_G81 N1549138 MID N1548992 MID -1
R_RL6 N1549138 MID R_NOISELESS 1
R_RL7 N1549138 N1549254 R_NOISELESS 10E3
C_C37 N1549138 N1549254 7.958E-13
R_RL8 N1549254 MID R_NOISELESS 7.407E3
E_E10 NOISE_OUT N1549078 N1549254 MID 1
I_I_B MID NOISE_OUT DC 300E-9
X_U3 MID NOISE_OUT VCC_B VEE_B IB_VS_VCM_OPAx863A
*R_R184 is NOT a noiseless resistor!
R_R184 MID N1573374 1E12
E_E8 N1573384 MID N1573374 MID 1.429E3
R_RL14 N1573384 N1573324 R_NOISELESS 10E3
C_C40 N1573384 N1573324 4.547E-11
R_RL15 MID N1573324 R_NOISELESS 7.005
E_E9 N1573556 MID N1573324 MID 5
R_RL16 N1573556 N1573332 R_NOISELESS 10E3
C_C41 N1573556 N1573332 1.592E-13
R_RL17 N1573332 MID R_NOISELESS 2.5E3
G_G83 ESDN MID N1573332 MID 1E-10
There appears to be a duplicate entry for Ib, as well:
I_I_B MID NOISE_OUT DC 300E-9
X_U3 MID NOISE_OUT VCC VEE IB_VS_VCM_OPA2863A
Finally, the model isn't available on the OPA863A product page, but only on the OPA2863A product page, and should be called OPAx863A (since it is used in either).
Older versions of PSPICE, and other simulators don't support "+" or "-" in subcircuit nodenames, these should be replaced with "plus" and "minus". And, they also don't support the "TC=0,0" syntax on resistors, which is especially annoying since the simulator default is TC1=0, TC2=0.
Regards,
Renan