This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA240-Q1: INA240 schematic consultation

Part Number: INA240-Q1

Tool/software:

Hi Teams,

Is there any problem with the design of the INA240A2QDRQ1 chip to achieve ground fault detection for two ground wires?

Please help review the schematic diagram,

thanks.

The principle is that when two ground wires are working normally, the current is about 40A, but when one of the ground wires is disconnected, the current of the ground wire becomes 80A