Part Number: XTR111
Tool/software:
I am using a PWM signal controlled by an ESP32 microcontroller to set VIN via a simple RC filter. I have been able to monitor the PWM signal and the VIN voltage and everything is tracking well. When I adjust the duty cycle of the PWM I get the appropriate voltage at VIN - scaled accordingly from 0 - 3.3VDC (please see schematic)

My issue is that the current measured at VLOAD (should be ILOAD) through a multi-meter does not appear to change no matter what the voltage at VIN is set to. I have attempted to measure the current with a 100 ohm series load resistor in circuit with the multimeter set to measure DC current (series load resistor not shown above). I am expecting a 4-20mA output over the range of VIN. However, the output current always seem to stay at roughly 39mA, though I do not believe this should be possible.
Looking for guidance as to what might be going on.
Thank you.