This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA860: Understanding the emitter current noise of the OPA860

Part Number: OPA860


Tool/software:

Hello all!

I am currently evaluating the OPA860 for an application where it would be configured as a common base amplifier and its noise performance is important.

Looking at the datasheet, I understand the noise specification I care about is the emitter noise current. Interestingly, in Fig. 23 of the datasheet I can see that this noise current increases for higher values of Radj, and thus that it decreases for higher bias currents.

I was surprised by this, as from what I understood from the internal structure of the OPA860 (from the datasheet as well as from section 2.3.6 of The Art Of Electronics), with its base grounded it would opperate basically as a complementary PNP and NPN common base circuit, where the classical tradeoff of Zin vs current noise would apply (i.e higher bias currents would mean higher gm would mean lower Zin but worse noise performance). Instead, it seems as with the OPA860 a lower input impedance and lower emitter current noise are achieved simulatenously!

Is this correct? If so, are there any tips anywhere how this is achieved? If not, what did I miss?

Thanks for any help!

Cai

  • Hi Cai, 

    I agree with you that the OPA860 architecture does not follow the typical expectation of a transistor. In the OPA860 the "transistor" portion of the circuit is what was referred to as a "diamond transistor" in earlier references. It is essentially a complex structure made of multiple transistors that can behave effectively like a transistor. Because this is a more complex design the OTA portion does exhibit noise correlations that are different than actual single transistors. 

    Best, 

    Jacob