Hi,
I need a fast VCCS that can put out 1.5 A. I was going to use the Cirrus PA09 but for external reasons
I can't use that package/part. I am thinking about using parallel OPA522 because that part is almost
fast enough but most of the suggestions around this technique use the other amps as slaves off a
single master amp. I don't see why I can't just use ballast resistors on a collection of OPA522 which
are having the same input voltage. I feel like the slave method will slow it down by the propagation
delay of one amp. My desired BW is at least 10 MHz and my desired slew is 10V/uS.
thanks,
steve