I'm looking for a long life surface mount substitute for the National Semi LMC6001. We're using it in an electrostatics monitoring application, so the most critical characteristics are the ultra-low input current specs. The LMP7721 looks like it meets or beats the LMC6001 in an SOIC package, except the supply voltage can only run up to 6V and our old design utilized the LMC6001 with a 12V supply. It doesn't look like a dealbreaker, but I was wondering if there are any other gotchas with the LMP7721 or if anyone has come across something comparable.
I've also looked at the INA116 which looks like another possible solution that would simplify some of our gain considerations, but looks slightly noiser.
Thanks,
Louis