Part Number: INA236
Other Parts Discussed in Thread: ISO1643, INA237
Hi Team,
From the datasheet of VIL, can I understand the maximum 0.4V means the threshold that regard as low will not exceed 0.4V? We measured the SDA low voltage level is about 450 mV, and INA236 didn't actually return Ack. Does this mean that the low level of SDA/SCL is too high?
In this thread it was written that "The input voltage must be 0.4 V or lower for it to be guaranteed to be read as low. The actual switching threshold will be higher, near 0.8 V, but there is no guarantee", but does that also apply to INA236?
Currently, we are using ISO1643 for isolation. When we connect the microcontroller and INA236 directly, communication is fine.
The INA236 is connected to the SDA1/SCL1 side of the ISO1643.
Do you have any other recommended isolation ICs?
Best regards,