This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM311 comparator

Hi

I'm using an LM311N comparator to switch a relay.  I have a single rail +12V supply.  I want to use it in a non-inverting configuration, so I have programmed a reference voltage at the inverting input of 50mV (240k and 1k potential divider from the +12V supply). The inverting input is connected (via 1k resistor) to a sense resistor (0.068ohms) in the ground return path of a load circuit.  My idea is that the comparator will activate the relay (connected between +12V supply and the comparator output) when the sense resistor current is greater than 0.75A or so. My thinking is that current > 0.75A will cause the inverting input to go > 50mV and drive comparator output low, turning on the relay.

But all attempts fail - the comparator output stays stubbornly high.

Is it not working because I am too close to the negative supply rail (i.e. 0V)?

I realise there are special purpose current sensing comparator devices, but I just wanted to mock up a prototype initially using some 311s I had to hand.

I have tried adding hysteresis (580k between output and non-inverting input), no effect.

Tony