Part Number: TRF37C73
Other Parts Discussed in Thread: DAC3482, THS9000, THS9001
Dear Technical Support Team,
I'm looking for OP1dB=20dBm(max) output with RF AMP such as Gali-84+(Mini-circuits).
TRF37C73 is 16.5 dBm (max).
Do you have any recommend RF AMP?
My configuration is below.
Max Power output: 20 dBm (6.325Vpp)
Frequency: 30MHz(min) and 250MHz(Max)
Input Voltage: 1Vpp form DAC3482(IOUTP/N → I/V →Transformer(1:1 , Differential to SingleEnd, 1Vpp max )→RF AMP→ 20 dBm (6.325Vpp) 50Ω load)
Best Regards,
ttd