Part Number: TLV1922
Other Parts Discussed in Thread: LM393LV
Hi,
I'm trying to use a single TLV1922 to detect undervoltage conditions of two 9V block batteries.
They're in series so I'm using an op-amp subtract circuit to get the top battery voltage referenced to the most negative potential.
Now the wording of the TLV1922 is a bit difficult for me to understand.
When both IN- and IN+ are within the common mode voltage range:
If IN- is greater than IN+ and the offset voltage, the output is low.If IN- is less than IN+ and the offset voltage, the output is high.If IN- is equal to IN+, the output state is technically indeterminite and output state is determined by the random polarity of the internal offset votlage.
So with a does this mean the output is active and asserted low or is the other way around?

(The +3.3V is referenced to -9V, not to GND)
Thanks!