Hello,
currently, I'm working on a project with low noise preAmp (need to sense signals about 200uVpp). I've been gave from my supervisor (I'm a 2nd year student of electronics) the LMH6624. The project requires an input stage (G = + 23 V/V non-inv), Sallen-Key LowPass on f0=4 MHz (G= 1 V/V) and output buffer (gain settable from a voltage follower to desired value). I send my schematic project in PDF (from Altium Designer 09).
My question is:
should I give RC between inputs of the filter and out buffer OpAmps (I assume, that I don't need to do that to the first stage casue of G=27dB)? And aroud what values should those RC be?
I know, that there are unity gain stable OpAmps but for now I need to use these.
Please help
Grzegorz Grzeda (PL)