Hey,
I'm now working on a trans impedance circuit using OPA4131(please see the following schematic), the bandwidth is set pretty low @ 330Hz, but the circuit oscillates (~3MHz) with a 10 meter long input cable (just a cable no sensor attached) which was measured having around 500pF capacitance. Then I intentionally tried C1 as 1nF (oscillating @ 1.6MHz, 2Vpp), 10nF (oscillating @ 330kHz, 4Vpp) and 100nF (no oscillation). All capacitors used are ceramic 0603.
It seems very weird to me because according to the application note "BOA055A", with the compensation capacitor C2 equals to 100nF, C1=500pF, 1nF, 10nF or even 100nF should be far away from the condition that would cause an oscillation. Because fz is around 160Hz~330Hz (very far away from the open loop bandwidth of OPA4131 which is 4MHz) and fp is very close to fz.
Could anyone help to explain what is happening to the circuit and why it's oscillating while it's not supposed to be? Thanks a lot!
PS: I tried a way cheaper MC33174 in the same circuit, 10 meter cable, 1nF, 10nF, 100nF all are fine, no oscillation at all. While the offset voltage is higher and not suitable for the application.
Regards,
Qi