Hello Dhruv and Collin,
Collin,
my intended application is similar to what Dhruv has explained where I need to give two 4-20mA loops using XTR115 or XTR116.
My loop power supply is of +24V and it is common for both XTR IC's.
In previous conversations regarding this I have learnt that the power consumed by the circuit in the input side of the XTR ic must be less than 4mA for two wire transmitter.
My input circuit should gets the power from Vreg pin of XTR116, But can you please explain the simplest ways to isolate two XTR circuits as the input to both the XTR is coming from same controller.
And how can I make Vreg pins of two XTR IC's common in case of getting more current like 4+4 = 8mA . (Please correct me if m getting wrong)
Regards
Shrikant.