Other Parts Discussed in Thread: XTR110, LM358, ISO122, TINA-TI, ISO124, LM7705, NE555, MAX232, LMC7660
Hello Collin,
Forum post referenced: http://e2e.ti.com/support/amplifiers/precision_amplifiers/f/14/p/135705/913927.aspx
I experienced the same problems with input ranges beginning with 0V
and output ranges beginning with 4mA.
But i need the complete 0-5V and 4-20mA range.
My source starts with 6mV but when i connect it to pin 5 it will be pulled up to 0,2V.
Over ~ 1 V all work fine and it is pretty linear. I use the circuit in FIGURE 1 and switch PIN 4 with PIN 5.
I read now in your post that i need a low-impedance driver for my input.
Can you please provide me with a tip how i can make from my (not so low impedance) circuit a
working low-impedance driver that is able to "short" PIN 5 to the 6mV? Maybe there is a IC that did the job?.
Best regards
Joerg