Other Parts Discussed in Thread: THS4131, ADS1271, THS4521
I am currently using the THS4131 as a driver for the ADS1271 much like figure 70 in the datasheet. However I now want to reduce power consumption and was looking at the THS4521, but the THS4131operates from a ±15V supply, the input signal is ±10V while the THS4521 operates from a single +5V supply. Essentially I need to attenuate my signal and drive the ADC while reducing power. Is it feasible to use the THS4521 in place of the THS4131 with the ±10V signal? If so, are there other component changes I need to make?