Other Parts Discussed in Thread: THS4631, TINA-TI, LM6171
Hi,
I'm having trouble changing the voltages at the supply rail terminals at high speeds. I'm using a THS4631 in the circuit below, where the supply rails of the op amp swing to follow the output. The rest of the circuit (not shown) has the op amp set up as a non-inverting amplifier with a gain of 15. VSS+ and VSS- are at 30 V and -30 V, though the rail-to-rail voltage should stay under 30 V with the resistor values below.
I would to run this at up to 1 MHz, but when I try to swing the rails to follow a square wave, they take a while to charge up to a higher voltage, even though the BJTs have a bandwidth of 10 MHz and are providing plenty of current.
We've ruled everything out except that the op-amp is causing this delay. So what exactly are rails connected to inside the op-amp? Is there some kind of capacitance inside that limits the voltage swing speed of the rails?