This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ref3012 output 1.25 to 1.32 in the circuit schematic

Other Parts Discussed in Thread: REF3112, REF3312, REF3212

Vref is ref3012, i need 1.25V output.

when Vin is floating or 0V, ref3012 outputs 1.25V.

when Vin is 3.3V, 5V or 15V,ref3012 output 1.32V.

i want to know whether i use ref3012 right. if ref3012 can't use in the circuit, can you give any advice for Vref.

Thanks very much!

Liang

  • Liang,

    REF30xx family including REF3012 can only source output current while its sinking capability is limited to only quiescent current of its output stage (-10uA) - see PDS table and graph below: 0mA < Iout <+25mA.

    For that reason applying Vin voltage above Vref results in erroneous output voltage since to bring the output to its nominal  value of 1.25V, REF3012 would have to sink the current coming from R2 pull-up resistor but it can't.

    We have other voltage references capable of sourcing AND sinking output current - please take a look at REF3112, REF3212, or REF3312.

  • Thank you very much. I replace for REF3112, and the circuit works well. The bad news is that our company will collapse.

  • Glad I could help. Good luck.