I have two questions about the OPA1S2385 which did not appear to be answered in the data sheet.
1) what are the electrical characteristics of the buffer section (op amp B) or does it have the same characteristics of op amp A (high bandwidth, FET input)?
2) What is the Quiescent Current of the entire OPA1S2385 device? The data sheet lists Quiescent Current: 9.2 mA (per amplifier). Does this mean that the entire device has a Quiescent Current of 18.4 mA, or does this current of 9.2 mA refer to the entire device with the buffer not counting as an amplifier?]