Hi
we use the Ina214 for current sensing in a motor controller, the setup is like the ti suggested circuit apart from the 2 following changes.:
1.ref voltage is set at 1.225v
2. Input filter resistor is changed to 1k instead of 0 ohm. ( the signal waveform is best at 1k)
i know that the ti data sheet has given a equation to calculate the gain error. But there are 2 problems really puzzling me.
1. The gain is only around 5 (tested) as compared to the calculated value.
2. With the exact setup on two exactly same PCB, the gain is different . (Output voltage error with the same current passing through shunt is around 100mV) Aren't they supposed to behave the same with the exact setup? Even with the gain error, the same setup should have the same error and why there isn't consistency in the same Ic setup?
The shunt resistor is 1.5m ohm /4. ( 4 connected in parallel)
1k input resistor 1%
we do need consistency and accuracy in our design , can anyone help us? Many thanks.
Frsnk