Other Parts Discussed in Thread: THS7347
Hello,
We are using THS7347 for buffered VGA output on our monitor. Actually we need two VGA outputs simultaneously. Is it possible to get dual output from THS7347 without I2C program?
And we are trying to write I2C command to this IC.
- IC's VDD and +VA are connected with +5V input.
- SDA and SCL are pulled up with 2.7K, and with 100E and 22pF RC filter as mentioned in datasheet.
- Both I2C address pins are grounded. So the slave address is 0x58.
For address transfer we didn't get acknowledgement from IC. Please check attached scope image of SDA SDL. What could be the problem. Please give answer to solve this issues.
Regards,
Bala