Hi all,
I'm now developing a system which combines two different types of sensors: ultrasonic and impedance sensors. In the system to achieve high-speed acquisition both of the sensors activated at the same time. For ultrasonic sensors I'm using piezoelectric transducer. The transmitted voltage signal is at 328kHz. For the impedance sensors the current excitation is 10mA at 150kHz. The problem is at the ultrasonic receivers the wave acquired are totally distorted as I activate the impedance current excitation. So far I have designed 2nd order band pass filter (centre freq=328kHz) but the problem still occurs. Attached is the images of the received ultrasonic signals when the current excitation is turn OFF and ON. Thank you in advance.
Pray for MH370
Fazlul