Other Parts Discussed in Thread: TLC274, TLV2374
Hello,
I had the following question come in about the TLC274AID and would appreciate the help.
"I’m analyzing a cct that someone no longer with the company designed for us because I’m not sure it has sufficient drive capability.
We use a TLC274AID quad op amp where each output drives a 350 ohm resistive load worst case. The signal is unmodulated IRIG and jumps between 5.8V for a mark and 0V for a space. The length of the marks and spaces are 2, 5 and 8ms. More detail here if needed: http://www.cyber-sciences.com/documents/TN-102_IRIG-B.pdf.
The signal spends 50% of the time high and 50% low. All 4 inputs are tied together so all channels drive high and low simultaneously. The amp power rails are +10V and -6V.
So, when the signal is a mark then 5.8V/350ohms = 16.6mA per output. The datasheet states that the max current per output is +/-30mA. 16.6mA is < 30mA so no worries there. However, Vdd max input current is 45mA and since 4 x 16.6mA =66.4mA > 45mA I’m suspecting I may have a problem. However, given that the signal is only driving 5.8V 50% of the and 0V 50% of the time I wonder if it’s safe to only consider the DC component of 2.9V for this analysis. If I do this then 2.9V/350 ohms = 8.3mA and 4 x 8.4mA = 33.2mA which is < 45mA and all is well.
Could you help a digital guy figure out if he’s got a problem or not?"
Let me know if you need any more information!
Thanks,
Eric