Other Parts Discussed in Thread: AMC1100, LM7705
Hi,
I use AMC1100 to measure high-AC voltage on 60Hz, all phases+neutral, as per attached schematics (please look below).To do preliminary tests, I used a waveform generator to apply 50mVpp/60Hz/sine between VinP and VinM. Then, I measured the output voltage of my AMC1100, between VoutP and VoutM: the voltage is 2.55V+200mVpp. Since I have 5V on VDD1 and 5V on VDD2, the DC value is as per datasheet. However, the gain is 4 only. Is there something wrong with my design?
The devices are marked as AMC11000-TI Z518-2AHG4. I have been told that G4 means Green-RoHs compliant, but I wonder if this could mean a special gain of 4 instead: my design is rather simple because the PCB must be as small as possible...
Thanks and Regards,
Etienne