This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL064: supply voltage missing min specification

Hello,

a question regarding the minimum supply voltage came up, as there is no clear specification of it in the datasheet but on the product page there is.

product page states: 7V minimum required total supply voltage

but: in the datasheet there are graphs with respect to supply voltage, which go down below 2V, which would mean a total supply voltage of only 3.6V or something like that.

I know the part is old, but still a clarification would be highly appreciated.

Thanks.