Hi All,
I am looking at a problem where I need to attenuate a large (+/-24V) signal for conversion, The INA143 looks to be a good choice for my problem.
I am looking at the effect of CMRR. The part has a minimum specified CMRR of 86dB. I have taken a look at this blog post [1] where there is a spreadsheet which performs the calculation. With a configuration of G = 10 and 0.01% resistor matching, the CMRR comes in at 88dB, essentially matching the datasheet. Fair enough.
When changing the configuration to G = 0.1 (my desired case) then the CMRR drops to 68dB, or about 360uV . This is quite a drop! Is there some difference in how the numbers are calculated vs the datasheet? What sort of voltage offset am I really looking at due to CMRR in this circumstance (e.g. 12Vcm because of the +24V - 0V difference)? How does this change compared to the G = 10 case?
Thanks in advance,
Damien.
[1] e2e.ti.com/.../what-you-need-to-know-about-cmrr-the-instrumentation-amplifier-part-2