Hi,
My customer needs the following information.
Could you show me the input--referred current noise of LMP2011 & TL061?
Thanks and Regards,
Kuramochi / Japan disty
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Tadahiko,
The LMP2011 is a "chopper" amplifier. The input pins will have large, pulsating currents in and out of the inputs.
You cannot really measure the "current noise" since it is buried in the noise of the charge injection due to the CMOS "chopper" switch noise. Therefore we could not measure it with any real accuracy. That line should have been removed. The LMP2021 datasheet explains this, and the weird dependance on input capacitance balancing.
You can think of the chopper noise as repetitive current noise (current pulses). The higher the input impedance, the more voltage is generated across the input impedance, and the worse the overall noise.
We do not recommend the use of the LMP2011 with source impedance of more than 1M Ohm. If the application is concerned with current noise, then the LMP2011 will not be suitable.
Art/John/Collin - did you ever publish the results of the your investigation of the chopper input pulses?
Regards,
Hello Paul,
Thank you for your information.
I confirmed the LMP2021 datasheet.
It indicates the input--referred current noise "350fA/√Hz".
I think that this current noise includes pulsating currents.
Is it corrct?
Thanks and Regards,
Kuramochi