Hi all,
Would you mind if we ask THS4520?
Our customer will use ADS58C28, and our customer would like to measure followings signal;
<Sampling signal>
-Input voltage range: 0-5V
-Input type: rail to rail
-Power type: single suply 5V
-Signal rate: 20Mbps
When they use ADS58C28, TI recommends LMH6552, THS4509 and THS4520 as ADC input driver(AC ,DC both).
These amplifiers don't correspond input range 0-5V, do they?
So, how about OPA2357 and THS4541?
If you have some advice, could you let us know?
Kind regards,
Hirotaka Matsumoto