What's the relationship between the low frequency cutoff and the value of the capacitor between pins COC1 and COC2?
Is it the bigger the capacitance the lower the cutoff frequency?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What's the relationship between the low frequency cutoff and the value of the capacitor between pins COC1 and COC2?
Is it the bigger the capacitance the lower the cutoff frequency?
Hello Minglai,
You are correct, a larger capacitor gives a lower cutoff frequency. On page 6 of the datasheet it states that the default frequency is 80kHz, but by adding a 330pF capacitor will reduce it to 10kHz. If you need a lower frequency you can use a larger capacitor. If the feature is not needed the two pins can be shorted.
Regards,
Loren