Hello. If we refer to XTR101 datasheet page 9, figure 5, we have seen a floating source e2' connected with proper input biasing with use of R2=2.5k. Now I wish to connect LM35 temperature sensor which is a fixed voltage source having Vcc, Gnd and Vout. How to wire it to XTR101 IC.? Mentioning input e1 pin 3 of XTR101 cant be grounded for single ended source because of linear response at 5V above pin 7. Please help me with some diagram.