I am using the LMH6624 in a high gain, non-inverting configuration with a gain of 51 (Rf = 499 Ohms, inverting input to ground resistor = 10 Ohms). Layout guidelines have been followed with ample ground plane in proximity to amplifier and cut out only under sensitive components and nodes. I am observing a very low level (< 10 millivolts) rf component between approximately 200 MHz and 300 MHz at the inputs and outputs, basically ALL OVER the circuit board. It seems impervious to changes in gain determining components. I am using a series 50 Ohm resistor at the non-inverting input. Aside from this low level spurious behavior, the desired signal pulse is being amplified correctly and I am filtering out the high frequency with a simple low pass filter.
QUESTION: What is the source of this spurious behavior? Is the the amplifier utilizing an internal chopper-stabilizing system to nullify offset or 1/f noise and am I observing residue of the chopper frequency ? The data sheet makes no mention of such a system but the amplifier is touted for ultra low noise and offset.
Thanks in advance for any help.