Dear all,
This is my first time on this support. I am a dutch student.
I have a INA2126 instrumentation amplifier used to amplify the results of a load cell. I supplied the amplifier with 5VDC and I have a reference voltage of 2.5VDC. The load cell uses a wheatstone bridge with two outputs that I feed into the INA2126. Typical output voltage of the load cell is 2.31VDC (both outputs). I have a gain of approximately 450. I have to research what happens when one of the two inputs get disconnected.
When I don't apply force to the load cell, the outcome of the amplifier is around 2.5VDC; which is to be expected. However, when I disconnect one of the two sensor outputs using a toggle switch, my output is amplified to the wrong rail (so I think).
An example:
O+ = 2.31V (sensor output one)
O- = 2.31V (sensor output two)
O+ is connected to Vin-
O- is connected to Vin+
When I disconnect O+, making O+ 0V, the amplifier output is pulled down to the negative rail (0V). However, I do notice that the output goes to the positive rail first and after a few millisecondes the output is pulled down to the negative rail.
When I disconnect O- instead of O+ than the effect is opposite. The output is first pulled down to the negative rail and after a few milliseconds the output is pulled up to the positive rail.
This is to me the exact opposite of what should happen. The output equation is (Vin+ - Vin-)*Gain + 2.5 ( (O- - O+)*Gain + 2.5 ). When O+ is disconnected, Vin- goes to 0V and the output should be amplified to the positive rail. When O- is disconnected, Vin+ goes to 0V and the output should be amplified to the negative rail. As my example above demonstrates, the real outcome is the opposite of what I would expect.
I found an article of a Texas instruments employee who defines the input common mode voltage range. He explains that the amplifier will not operate linearly when outside the input common mode voltage range. The input common mode voltage is given by (Vin+ + Vin-)/2. When both sensor outputs are connected, the input common mode voltage is 2.31VDC. When one of the two sensor outputs is disconnected, the input common mode voltage should be 2.31/2=1.155. In the INA2126 datasheet, i see the graph for the input common mode voltage range and its corresponding output. An input common mode voltage should be greater than 1VDC. When disconnecting one sensor output, I do approach the minimum of the range but I should stay within the correct range.
Article: http://www.planetanalog.com/document.asp?doc_id=528175#msgs
I am having a real trouble understanding why this occurs. Do I exceed the input common mode voltage range which would explain non-linear behaviour? Or is there something else that I am missing?
Hope to hear from you guys soon.
Thank you in advance.
Kind regards,
Gijs de Vries
Student