Hi,
I want to build a receiver with a photodiode. First I set up a circiut with OPA381 and I used 10K ohm feedback resistor. It worked well with its gain of 10K. But then I wanted a faster one and decided to use THS3202. I tried to amplify in two stages. First one as TIA had an Rf of 500ohm and second as non-inverting amp had an Rf of 500ohm and 26ohm to GND. So it had a gain of 500x20=10K. But I did not get a meaningful output. What should I do? Do I need a different op-amp?
Thanks,
Emre