Is there any data on output impedance vs frequency for LMH670x?
The datasheets don't seem to have any graphs.
What I'm looking for is a buffer that has low input impedance (<1.6 pF, preferably 1 pF), noise <5 nV/sqrt(Hz), 500 MHz BW with 1 Vpk-pk pulses or better, and output impedance of only a few ohms up to 100 MHz & reasonably flat (for easy termination in 50 ohm system). Clean pulse response with little overshoot is required, and settling time to 0.1% <10 ns (faster is better, but overshoot has to be at most few %).