Hi,
I'm trying to use delay circuit as given in datasheet of LMH6628 (shown below) . I'm using a input pulse of 5V amplitude. R and C are 41.2 ohm and 33 pF respectively. + Vcc is 9V and -Vcc is 0V for both LM7121 and LMH6628. The output of LM7121 is fine. However, the amplitude of output of LMH6628 at pin 3 and pin 7 is around 200-250 mV. The output of delay circuit is connected to a inverter which in turn is driving an optocoupler. Could anyone advise what might be wrong?
Thanks