Other Parts Discussed in Thread: OPA2171, LM2904, TINA-TI
dear supporting team,
is there clamp circuit btw IN+ &IN- of OPA2171? customer found when the input voltage difference btw IN+ & IN- is very big, then IN+ and IN- will affect each other. tks!
The issue phenomenon is as below:
PIN3 is input of 2.5V reference through 1K Ohm.
PIN2 is the voltage sampled & amplified from output current(OCP)
1. if using OPA2171 in D2, when the brd is unloaded, they will find the voltage of PIN3 is only 2.15V, when output current is increasing, i.e PIN2 voltage will increase as well, PIN3 voltage will also increase. when output current get to 30A, then PIN3 get to 2.5V. then even they increase the output current, PIN3 keep 2.5V.
2. if remove R125 and C13, pin2 is floating, PIN2 is not 0V.
3. if change D2 to LM2904, keep other portion the same. PIN3 will stay at 2.5V, will not change with the output current. so what cause the different behavior of LM2904 and OPA2171?