Other Parts Discussed in Thread: OPA637
Dear Forum,
I am trying to implement a typical transimpedance amplifier to amplify the current from a photodiode using an OPA637, as shown below. However I am getting rail to rail square wave oscillations. I am powering the circuit with plus/minus 12V batteries, which should be very quite. The oscillations occur at a wide variety of Rf (2K Ohm, 20K Ohm, 100K Ohm) and a wide variety of feeback capacitors across Rf (5 pF, 18 pF, 100 pF, 1800 pF). The largest capacitor turns the output into a triangle wave. Removing the photodiode makes no difference. The circuit is perfectly well behaved when I substitute the OPA637 with OPA128. What am I missing?
Adriaan