Part Number: INA194
Other Parts Discussed in Thread: INA282, INA213
Hi Team,
I have a customer who is using the INA194 and had a question about the operation of the INA194 in the Low VSense mode as specified on page 19 of the datasheet.
In the case when VCM is 20V and VSense is <20mV, the INA194 is specified to have a maximum output voltage of 300mV. The questions are:
1. Is this value of 300mV specified over the entire temperature range? How would temperature affect this value?
2. How stable is a this specific offset Voltage over the lifetime? Can you specify the deviation of the value? Is it possible that this voltage would increase or decrease over the lifetime of the product?
Regards,
Mihir Gupta
FAE - South Germany