Part Number: ONET8551T
Under the condition of different optical input power,when shutdown the input signal,there are different output waveform;as below
RX=-1.0dBm
RX=-5.0dBm
RX=-10dBm,
rx=-15dBm
Questions as follows
1.Under the condition of different optical input power,why the output waveform delay time is different(from max amplitude to min amplitude);the max and min delay time is how much microsecond?
2.in the case of having normal optical input signal, the max amplitude value of output waveform is how much?
3.if shutdown the input signal,whether the output waveform amplitude value is more and more smaller?
4.when RX=-15.0dBm,the output waveform with a little more slowly up and down, why such a phenomenon?
Urgent looking forward to your reply,many thanks!