This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA132: INA132 about the design question

Part Number: INA132
Other Parts Discussed in Thread: OPA2191, INA826, INA126

Hi Team,

The customer would like to use the op amp to design his circuit. The input signal is 0~20mV and it is 100HZ. 

After the signal is  amplified by the op amp, the output voltage must be -10V to 10V. 

My idea is the customer may use INA132 for the differential amplification. 

First, the customer may give a 10mV reference voltage as the input voltage for INA132. 

Then the output voltage for INA132 can be from -10mV to 10mV.

Finally, the -10mV~10mV voltage can be amplified 1000 times to reach -10V to 10V. 

Q1: Is my idea correct? 

Q2: If my idea is correct, is INA132 suitable for the customer's application?

When the -10mV~10mV voltage is needed to amplified 1000 times to reach -10V to 10V, which op amp can be suitable?

Best Wishes,
Mickey Zhang
Asia Customer Support Center
Texas Instruments