Part Number: LM139
Other Parts Discussed in Thread: LM397
LM139
The datasheet for this part states that the input common mode voltage can range from 0 V to VCC– 2 V. It also describes the outcomes of input voltage ranges that exceed this common mode range as follows:
• When IN– is higher than common mode and IN+ is within common mode, the output is low and the output transistor is sinking current
• When IN+ is higher than common mode and IN– is within common mode, the output is high impedance and the output transistor is not conducting
• When IN– and IN+ are both higher than common mode, the output is low and the output transistor is sinking current
Please confirm:
• whether this is guaranteed (or typical) operation of the device.
• my interpretation of the datasheet is that the device input voltage can exceed the supply rails. Is this correct? If so, please confirm what feature of this device makes in unique from other comparators that limit the input voltage to the supply rail.
• exceeding the common mode range of the device will not cause damage as long as the input voltage is within absolute maximum rating of -0.3 to 36V (stated in datasheet). If this is not the limit, please state the maximum input voltage that this device can withstand without damage.
• What is the maximum voltage rating for transient voltage <200us? Particularly, I am interested in the lower limit of –0.3V. Can this device withstand –1V for duration <200us without damage?
• please confirm that allowable input voltage range when the LM139 is supplied with +/-12V rails.
• do your responses above apply to device LM397?