Other Parts Discussed in Thread: TL971,
I am stumped.
This is a quad opamp wired up with a single supply (0,5VDC), feeding into the positive is the output from a DAC(no resistor, straight connection). The output is fed back into the non-inverting with no caps or resistor. It is the simplest form of a voltage follower, just like Figure 17 on the datasheet although it is not a 12V rail rather a 5V rail.
When DAC output is 4.9V, (input to ch1+) voltage follower output is 4.9V (expected), when DAC output is 0V, opamp output is 1.7V, (not expected)
I have debugged the circuit and now only have exactly as described. There are no other signals ensured though a liberal cutting of traces to isolate the problem.
To be double sure, the +input of the opamp was hard grounded and still results in a 1.7V output.
I'm at a bit of loss as to what is going on. The wiring does not get any simpler than this, power is solid 5V, ground is a solid 0V, DC signals.
Double checked wiring and PCB layout, double checked that bug is in correctly, This problem occurs on all 4 channels as well as a second PCB. At least it is consistent.
Any suggestion on what could be happening here?