Part Number: INA230
Other Parts Discussed in Thread: INA240
Hi,
INA230 About input sink current
In the circuit that measures the shunt voltage. (It is not Bus voltage measurement)
Do not connect a shunt resistor between IN+ pin and IN- pin,
When 0 V is applied directly to the IN+ pin and +15 V to the IN- pin,
Will the leakage current of the IN- pin be significantly larger than 10 uA (TYP) of the data sheet?
With this circuit configuration, a current of about 1.7mA flows through the IN- pin.
best regards