This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV3541: AD8615AUJZ-R2 Replacement Availability

Part Number: TLV3541

hi

I am trying to replace the AD8615AUJZ-R2 with TLV3541IDBVR.

We will contact you as an alternative part.

(1.8V 115mA_max, 3.3V 95mA_max, 5V 50mA_max variable power rail will be used.)

The current specification can be lowered slightly.

In terms of bandwidth, the ADI product is 20MHz, while the TI product TLV3541IDBVR is 250MHz.