I am using REF3012AIDBZT as a voltage reference.
The input is 3.3V but output is 1.78V instead of 1.25V.
I have checked purchasing bill, it is REF3012AIDBZT.
What is the problem?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using REF3012AIDBZT as a voltage reference.
The input is 3.3V but output is 1.78V instead of 1.25V.
I have checked purchasing bill, it is REF3012AIDBZT.
What is the problem?
Thanks.
Hi David,
Can you share your REF3012 circuit configuration with us? Make sure that the device has the R30A marking on the package. Also, if you have an O-scope available, take a look at input and output pins and make sure that all you see are DC levels.
Regards, Thomas
PA - Linear Applications Engineering