The datasheet for the OPA227U precision op amp indicates that the offset voltage can be trimmed using the circuit shown on page 11 ( doc# SBOS110A).
Can you tell me which direction the offset changes when the resistance between pin 1 and V+ is increased?
For example, if the resistance from Pin1 to V+ is 5K, and the resitance from pin 8 to V+ is 15K, will the offset voltage be higher than when the wiper is in the middle of the trim resistor?