This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV9004: suitable for DACs?

Part Number: TLV9004
Other Parts Discussed in Thread: DAC124S085, LM2776, , OPA192

I'm using the TI DAC124S085 with a 3.3V supply as a 4-channel 12-bit DAC driving up to about 200mA total, operating at frequencies up to 10kHz.  I want to operate a rail-to-rail amplifier in a bipolar setting (with the TI LM2776 switched capacitor inverter providing the -3.3V), as shown in section 9.2.1 of the DAC124S085 datasheet (http://www.ti.com/lit/ds/symlink/dac124s085.pdf.  The design is highly space and cost constrained.  Is the forthcoming TLV9004 well suited as the quad op amp for this DAC?  It seems like it might be, but DAC is not listed on page 1 of its datasheet as a typical application (I know this is not an exhaustive list though...).  Is TI still looking at large-scale production towards the end of September?