This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA286-Q1: Use INA286 to detect 0.1mv

Part Number: INA286-Q1
Other Parts Discussed in Thread: INA286, TLV313,

I would like to detect 0.1mv--20mv of a 2mohm R(current is 0.05mA~10A),

the INA286's output is 10mv--2v.  The AMC1211's output is (1.44-1~1.44+1),

the TLV313's output is 1.5*(0~2)=0~3v  , this will be transmit to mcu's 12 bit ADC(3.3v power). 

I am not sure if it works ,or I should use a 10mohm R instead , then the detect current scope  will redued to 0~2A

 

  • It should be 0.1mv--20mv of a 2mohm R(current is 0.05A~10A)
  • Hello Liang,

    Thanks for considering to use Texas Instruments. The calculated outputs you have for each stage of your circuit look correct. However, the INA286-Q1 could present an undesired degree of error at 0.05A. This would be due to the offset voltage referred to the input. As your ideal expected minimum Vsense would be 100uV and the typical offset is +-20uV, you could have a 20% error or even as high as a 70% error from input offset alone. Do you absolutely need this resolution? If so, you could use a larger resistance as you suggested above. Perhaps you could use two shunts in parallel to get a 5mohm resistance. Are you expecting the common mode to your current shunt monitor to go well below 0V?
  • Hi Patrick 

      Yes,  there is another circuit to detect current under a negetive common voltage of -12.6v, so I select INA286,  the GND of 6 battary seris is on the middle position.  If I use a low side current  detect on the GND position, the current maybe bidirection